Density

Recent posts

  • best-practices-for-data-center-rack-resiliency-in-ai-environments - https://cdn.buttercms.com/3D40YfbzSIqLy8MAfhke

    Best Practices for Data Center Rack Resiliency in AI Environments

    Rack Power
    July 31, 2025

    As data centers deploy high-density servers and equipment to support power-hungry artificial intelligence (AI) workloads, they must ensure that racks are resilient, and operators can manage them safely.


  • understanding-u-space-and-why-its-important - https://cdn.buttercms.com/SRI37lRRTRm8k37D85Rv

    Understanding U Space, and Why It’s Important

    Rack Power
    June 16, 2025

    Data center racks are measured in rack units (RU), commonly abbreviated to U. One U measures 1.75 inches and is used to define the amount of vertical space available in a rack. Knowing what U stands for is critical for data center planning because it standardizes rack and gear height with a uniform measure.

    • Categories:

  • driving-data-center-efficiency-with-high-density-rack-pdus - https://cdn.buttercms.com/oVIDuaddRWj6O96GTzcs

    Driving Data Center Efficiency with High-Density Rack PDUs

    Rack Power
    May 28, 2025

    Energy efficiency is a top priority for data centers. Power demand is surging, driving a sharp rise in rack densities—and with it, the need for high-density rack PDUs to reliably support advanced computing workloads.


  • data-centers-are-getting-denser-and-smarter-heres-how-facility-managers-can-keep-up - https://cdn.buttercms.com/tJYMs582Qce91wtRBxXp

    Data Centers are Getting Denser and Smarter: Here’s How Facility Managers Can Keep Up

    Elie Byrne
    May 29, 2024

    Data centers are under pressure to adapt to the demands of emerging technologies. As a result, data center operators will need to rethink existing facilities and design new ones to accommodate higher density, greater efficiency, elevated reliability and resiliency, and enhanced sustainability.


  • may-the-pops-be-with-you - https://cdn.buttercms.com/ysmknNMrTUm4z6k6re0F

    May the POPS Be with You

    RJ Tee
    December 13, 2017

    Since much of the buzz this week will be about the much-anticipated release of Star Wars ‘The Last Jedi’ on Friday (or Thursday if you happen to live in the UK), we thought we would take a moment to share some of our favorite old lines. And now, from a galaxy far, far away… (cue fanfare) “The force is strong in this one.” Bad guy or not, Darth Vader hit the nail on the head here. While we had to wait until much later to find out why he knew what he knew, we do know now that sometimes you just have a feeling about things. The Server Tech team had that same good feeling when we started talking about ZTP, our zero-touch provisioning approach for our PDU line. (We even have a pretty nifty whitepaper...) A way to provision all your rack mounted power strips at once, hands-free, and outside of the data center? We still have to remind people this is no Jedi mind trick.

    • Categories:

  • where-density-square-meters-and-practicality-meet - https://cdn.buttercms.com/qdBoNPfKS8SI8ujxQ1tL

    Where Density, Square Meters, and Practicality Meet

    RJ Tee
    August 03, 2017

    In this recent article on Data Center Knowledge, the author discusses the growing issue of data center real estate in Singapore and other APAC markets – or more accurately, the lack thereof. While many countries, including portions of the United States and Northern Europe, benefit from large landmasses, high-density city centers in most of the world place an absolute premium on every square meter of space. In these areas, data center facilities are built more on the vertical axis, with support equipment stacked on rooftops and in basements.

    • Categories:

  • low-on-real-estate-high-on-rack-components - https://cdn.buttercms.com/CpdZcwYIR0Gq9VNvQcWG

    Low on Real Estate, High on Rack Components?

    Josh Schaap
    December 05, 2016

    You need High Density Outlet Technology (HDOT) PDUs from Server Technology, which can support more rack components than any other PDU per form factor. To combat the limited physical space that PDUs compete for in the data center rack, Server Technology developed High Density Outlet Technology (HDOT), the smallest form factor PDU which significantly increases real estate in the back of the rack by fitting as many as 42 C13’s in a 42U high network managed PDU device—that’s over 20 percent smaller than a comparable PDU using standard outlets. In conjunction with the launch of HDOT, Server Technology developed a quick turn manufacturing process that provides short lead times for PDU’s with the exact combination of C19 and C13 outlets in the locations where the customer needs them. The HDOT design also provides high native cord retention of over 12 pounds pull strength, reducing or eliminating the need for custom and costly ancillary locking cord devices. With increasing outlet density comes increased power, and potentially increased heat. HDOT is manufactured with robust high-temperature materials carrying a UL94 V-0 flame rating, making these outlets ideally suited for the harshest data center environments

    • Categories:

  • shouldnt-we-be-talking-about-medium-density - https://cdn.buttercms.com/Xr9lhGsSSrO89Vi4RuXo

    Shouldn’t We Be Talking About Medium Density?

    RJ Tee
    October 16, 2016

    In the world of rack-mountable power distribution, the term high density is so hot right now. After all, it is no secret to anyone in the industry that the business that takes place within the four corners of a rack has been warming up faster than a Jane Fonda workout video.

    • Categories: