Cisco
Server Technology Application Notes for powering the Cisco Unified Computing System
As power densities increase planning and implementation of the required amount of power to ensure proper operation and redundancy is critical to success of any server installation. For example using a Cabinet Power Distribution Unit instead of running power in-feeds directly to the servers can save tens of thousands of dollars in installation and operation costs throughout the life of the devices.
Listed below are application notes showing how to properly power and provide for redundancy various configurations of the Cisco UCS 5108 Series Blade Server Chassis, Cisco UCS 6120XP 20-Port Fabric Interconnections and Cisco 3845 Integrated Services Router utilizing Server Technology Inc. Cabinet Power Distribution Units (CDU’s) with various power in-feed types based on the required amount of power for each system.
The Cisco Unified Computing System is a next-generation data center platform that unites computing, network, storage access, and virtualization into a cohesive system designed to reduce total cost of ownership (TCO) and increase business agility.
Cisco Unified Computing System - Deployment at Northern California Data Center
208V 30 Amp Scenarios - Cisco Unified Computing System and Server Technology Smart CS 12HD2-L630 PDU
208V 30 Amp Scenarios - Cisco Unified Computing System and Server Technology Smart CS 24V2-L30MA PDU
Two Cisco UCS 5108 Chassis, One Cisco UCS 6120XP 20-Port Fabric Interconnects with Server Tech Smart 24V2-L30MA
3-Phase 208V/120V 60 Amp Scenarios - Cisco Unified Computing System and Server Technology Smart CS-18VYY813A2 and CL-18VYY813A2 PDU
Three Cisco UCS 5108 Chassis and Two Cisco UCS 6120XP 20-Port Fabric Interconnects
Four Cisco UCS 5108 Chassis and Two Cisco UCS 6120XP 20-Port Fabric Interconnects
Five Cisco UCS 5108 Chassis and Two Cisco UCS 6120XP 20-Port Fabric Interconnects
Six Cisco UCS 5108 Chassis and Two Cisco UCS 6120XP 20-Port Fabric Interconnects
3-Phase 415-240V 30 Amp Scenarios - Cisco Unified Computing System and Server Technology
Smart CS-24V5Z311 PDU
Three Cisco UCS 5108 Chassis and Two Cisco UCS 6120XP 20-Port Fabric Interconnects
Four Cisco UCS 5108 Chassis and Two Cisco UCS 6120XP 20-Port Fabric Interconnects
Five Cisco UCS 5108 Chassis and Two Cisco UCS 6120XP 20-Port Fabric Interconnects
Six Cisco UCS 5108 Chassis and Two Cisco UCS 6120XP 20-Port Fabric Interconnects