rack pdus

Recent posts

  • I33ikimhrzal4een8gyw

    Using a Horizontal vs. a Vertical Rack PDU

    Posted by RJ Tee on October 19, 2017

    While use of vertical PDUs, or vertical rack power distribution units, has become nearly ubiquitous in today’s data center, they are not the only game in town. Since we have been getting a lot of questions lately about Horizontal rack PDUs, we thought it would be useful to take moment to pause and reflect on our counterpart from the other axis. Besides orientation, the most obvious difference between the two rack mount power strips is that of space – outlet space to be exact. Since the typical horizontal PDU fills 1 to 2U gaps, the number of outlets available is limited to the width of the rack, or the number of U spaces you are willing to part with.


  • Gjvqkb23tti0b5lswjgb

    Spectre and Meltdown vs. Servertech Rack PDUs

    Posted by RJ Tee on March 01, 2018

    Server Technology has you covered when it comes to threats from the latest cybersecurity attack. Like last week’s YouTube star, the latest security threat has come and gone. It is unfortunate that these attacks have become so commonplace that they barely raise an eyebrow these days. I imagine that this is much to the chagrin of the nefarious code writers who are cooped up in an abandoned warehouse in a very, very cold part of the planet hacking away right now.

    • Categories: