Industry Trends and Solutions

Recent posts

  • Hxkyknngsd3ufabuwgql

    What’s the Best PDU Solution?

    by RJ Tee

    There are a lot of best PDUs, then, and that is the point. The goal of our product line and the design of our manufacturing process is to allow our customers the ability to find exactly the right set of power distribution features for their application. Why else would Server Technology provide so many options, from horizontal to vertical, 120V to 415V, low density to high, and from managed to not? It is because every data center rack is its own unique deployment, which demands the ultimate in flexibility from those devices that power the load.

    Categories: Server Technology

  • J8kxwsz0rzeso0fhaymj

    The Dynamic Data Center: Driving Lower PUE

    by Kayla Poole

    In support of the new Marc Cram white paper, “Flexibility and Sustainability for the Dynamic Data Center,” we are going to be rolling out a three-part blog series that supports some of the key data center themes covered in the document. The paper itself, a copy of which can be found here, is a mission-critical state of the union address that calls attention to the challenges facing today’s dynamic data center operators.

    Categories: Server Technology

  • Sc2ibcn9q2mvdzltsg3w

    Managing the Challenges of Density

    by Josh Schaap

    When considering implementing a power-dense data center, you face a number of challenges: cost, heat, load balancing, data center environmental monitoring and power monitoring, increased network traffic and system configuration management. With each of these challenges come serious, seemingly insurmountable obstacles, but with the proper planning and understanding, it can be done. As the Power Strategy Experts, Server Technology is here to help you successfully manage density and data center power.

    Categories: Server Technology

  • Lp6xwgstdee5aklqouwe

    Five Major Costs of Data Center Downtime

    by RJ Tee

    Data center downtime is one of the most expensive threats facing IT professionals today. The overall cost of downtime can range from thousands of dollars per minute to hundreds of thousands of dollars per hour, depending on the size and severity of the outage.

    Categories: Server Technology

  • 2n9fsgx0qrcm1ywcwlyu

    Are You as Resourceful as Mark Watney in ‘The Martian’?

    by RJ Tee

    In the Oscar-nominated film “The Martian,” astronaut Mark Watney, played by Matt Damon, uses his wits and available resources to attempt survival on a hostile planet. With a limited supply of food, water and air to breath, he optimizes his immediate resources to mitigate risks posed by the dangerous forces surrounding his space station.

    Categories: Server Technology