Server Technology Inc PRODUCTS   :   USING SENTRY   :   COMPANY   :   RESELLER
Remote Power Management Come See Us!
What's New
Downloads

NEW Sentry POPS (Per Outlet Power Sensing) and SPM Sentry Power Manager

To reduce power consumption and maximize each cabinet installation, more information is needed, per device, per application, per cabinet, per groups of cabinets and per facility. The ability to monitor the power load of an individual outlet within a Cabinet Power Distribution Unit (PDU) opens the door for significant opportunities to monitor and maximize efficiency, plan for future installations, determine the best location to allocate additional cooling resources and identify idle devices that are candidates for virtualization or to be shut down.

SPM combined with POPS allows power monitoring at the outlet level. This provides the Data Center Manager kW and kW-h information per device, groups of devices (application) an individual PDU or cabinet. Utilizing SPM's exclusive "clustering" technology allows power monitoring across individual IP addresses providing kW and kW-h power information across multiple cabinets or the whole data center.

SPM provides a central interface capable of managing and monitoring thousands of Sentry Cabinet Power Distribution Units (PDU's) in multiple locations for conditions including:

  • Power, temperature and humidity monitoring.
  • Monitor current voltage, power(kW), apparent power, crest factor and power factor.
  • Real time status and alarm notifications viewed by their status. 
  • Trending of critical parameters such as temperature, humidity, in-feed load, in-feed power, system watts/unit area, kW, kW Hr, and system total power.
  • Power information for the user to create custom graphs based on any one or all of these parameters.

This information can be used to calculate "green" power efficiency metrics like PUE and DCiE offered by The Green Grid.  Beyond calculating efficiency metrics this technology also provides the ability to bill for power usage based on an individual outlet, device, groups of devices (application), cabinet, groups of cabinets or the whole location. 

Server Technology to exhibit at Upcoming Technology Convergence Conference.

Held on February 19, 2009 at the Santa Clara Convention Center in Santa Clara, CA. Get a head start for 2009 and discover the latest advancements in IT Infrastructure, Telecommunications, Security, Wireless, and Networking. Gain key strategies to effectively deal with the top issues and trends in your mission critical environment today.

For more information on the Technology Convergence Conference click here.

Server Technology Announces New Switched Products

Two New Mixed Outlet Switched Products from Server Technology:

CS-36VD/VY-3Ph
The CS-36VD/VY-3Ph is a 3-Phase, 208V product with (24) C-13's and (12) C-19's. It is available in 60 Amps as a Delta or Wye unit configuration.
For more information on this product click here.

CS-18VD/VY-3Ph
The CS-18VD/VY-3Ph is a 3-Phase, 208V product with (6) C-13's and (12) C-19's. The unit is high density with a rated amperage of 60 amps.
For more information on this product click here.

Upcoming Trade Shows

Server Technology will be exhibiting at domestic and international industry shows in 2009.  These shows are an excellent opportunity to discuss your data center goals and objectives with our Server Technology representatives.

For more information on upcoming shows click here.

Server Technology Sales & Marketing

 
 
Server Technology, Inc.
Global Headquarters
1040 Sandhill Dr
Reno, NV 89521
1.800.835.1515
www.servertech.com
www.servertechblog.com
E-Mail: sales@servertech.com
Server Technology, Int.
EMEA
Sienna Court
The Broadway
Maidenhead
Berkshire
SL6 1NJ United Kingdom
Tel:+44 (0)1628.509053
E-Mail:
salesint@servertech.com

Server Technology, Int.
APAC
37th Floor,
Singapore Land Tower
50 Raffles Place
Singapore 048623
Tel: +65 6829.7008
Fax: +65 6234.4574
E-Mail: salesint@servertech.com