White Papers
NEW! Efficiency Gains with 480-277V Power at the Cabinet Level
This paper explores the merits and drawbacks of 480V/277V power distribution versus the more conventional 208V and 415/240V 3-phase designs in use today. At present there remains a number of challenges associated with implementing 480V/277V at the rack level that will need to be overcome before sales volume of 277V gear is sufficient enough to reach price parity with the acquisition and operating costs of 415V/240V infrastructure and products.
NEW! Advantages of Wire-Free Power Monitoring in the Data Center
When RF Code Sensor tags are used in conjunction with Server Technology PIPS and POPS CDU's, the solution is a world class wire-free power monitoring solution right at the rack or cabinet level.This article explores how this solution works, and how it can help you improve your data center.
Cabinet Power Monitoring, Management & Control Within the Data Center
This article explores the various monitoring systems typically found within the data center ecosystem and how to navigate getting the required power and environmental information needed to make better decisions within your data center facility.
Phase Balancing: The Last Few Inches Of a High-Efficiency Power System
This paper discusses the effect on efficiency of load balancing across phases in a 3-phase distribution system.
Power Efficiency Gains by Deploying 415 VAC Power Distribution in North American Data Centers
Power densities within the cabinet continue to rise and result in a rising demand for 415 V products in North America, once a solution only considered internationally.
Measuring Power and Efficiency
"Green" Data Center Using POPS for outlet power sensing and Sentry Power Manager.
Planning, Implementing and Application of Cabinet Power Distribution Units
As businesses and organizations plan for the next decade and build out their data centers, power consumption and distribution to the devices in the cabinet must be taken into consideration early on in the planning stages.
3-Phase Power in the Data Center
3-Phase power demand in the data center equipment cabinet.
Cabinet Power Distribution Solutions for Critical Environments at Colliers Turley Martin Tucker
The type and amount of power delivered to the cabinet can greatly affect costs, cooling efficiency, redundancy and future expansion plans within their facilities.
Smart Load Shedding Ensures Uptime
Zero down time is the key driving factor in today’s data center design and operation; Smart load shedding allows the operator to automatically shed designated, non-critical, devices.
Features & Benefits of Implementing Server Technology's Cabinet Power Distribution Units (PDUs) in Your Data Center
Metered, Smart and Switched Cabinet PDUs provide many solutions to common data center problems including cable management, temperature and humidity monitoring, circuit overload prevention and remote reboot capabilities, and many others.
Article "Circuit Breakers - Are you protected"
Differences between using fuses and circuit breakers in providing overcurrent protection in a Cabinet PDU.
JITC tested PDUs for DOD IT and NSA Applications
The Joint Interoperability Test Command (JITC) is the independent evaluator for information systems for the Department of Defense (DOD); the JITC is responsible for conducting Information Assurance (IA) and Interoperability (IOP) testing of network devices that will be connected to the Global Information Grid (GIG).
Cabinet Level Power Distribution Solutions for High Density Cabinets
Denser cabinets requiring more power and cooling continue as the trend for Data Center cabinet installations.
Branch Circuit Protection in Cabinet PDUs
Branch Circuit Protection plays an important role in UL 60905-1 certification for Data Center equipment.
Best Practices for Secure Remote Power Management
SSL & SSH Security for Protection of Remote Management of Cabinet PDUs.
Maximizing Network Uptime - Positive Impacts of Remote Power Management
Sentry Remote Power Manager and reboot (power cycling) features.
True RMS Input Current Monitoring
True RMS input current monitoring can be utilized to calculate and forecast power in the Data Center at a cabinet level.
Who Needs -48VDC Remote Power Management?
–48 VDC Remote Power Management for routers, ATM switches, and DSLAMs.