Server Technology Inc Products   :  Support  :  Using Sentry  :  Company  :  Channel Partners  

 

Using Sentry

     








   
Home  >  Using Sentry  >  Sentry Switched CDU Online Demo

Sentry Switched CDU Online Demo

This Server Technology Sentry Switched CDU Online Demo consists of two horizontally mounted CDUs, each with 8 user manageable outlets (model numbers CW-8H1-C20 and CX-8H1-C20). These two units are linked in a Master/Expansion configuration so that the two units function as one and share one IP address with all 16 outlets displayed under one login.

In the Demo, the outlets from the Master unit are numbers .A1 for Outlet 1, .A2 for Outlet 2 and so on. For the Expansion unit, Outlet 1 is labeled .B1, .B2, etc.

Features of the Switched CDU Products   

 

 

  • Easy to use and access, secure, integral HTML Web GUI over HTTP/S, plus LDAP/S and TACACS+ external authentication and authorization support
  • Secure remote power management; reboot individual or grouped outlets (SSL, SSH, Telnet, SNMP, RS-232)
  • Outlets may be linked to one or multiple groups without loss of control of that individual outlet
  • Native power-up sequencing prevents in-rush current overload during initial start-up or after power loss.  Unlike other products on the market, sequencing occurs during initial startup, after power loss and after user-initiated power cycling to prevent overload
  • True RMS input current monitor(s) on easy-to-read local LED, via network or serial connection
  • Optional temperature and humidity probes with 10-ft cords to allow sensors to be located in different locations
  • SNMP traps provide automated alerts for power and environmental conditions.  Additionally, event notification is available via Syslog and email
  • Expandability: add additional outlets under one IP address through link unit
  • Local and remote notification if a branch circuit is down (FE will display on LED and through the web-based interface, SNMP and email alerts)
  • 3 Phase products have a separate LED for each phase to simplify load balancing 

    Fuses
    Fuse Retractors available on certain CW/CW vertical models

    Linked_units-Server Technology
    Linked Master and
    Expansion Units

    LED_Network_Serial
    LED current monitor.
    Ethernet, Serial and temperature/humidity ports

    Web Interface Demo
    »Click here to begin HTML Demo

    At the authentication page, enter the following:
    Username: admn
    Password: admn
    Click on 'OK'
    To logout, click on the link located in the navigation bar on the left of the screen. 

    Product evaluation checklist

    In order to maximize the demo and fully understand all the features of the Switched Products check out the CW product evaluation checklist 

    Telnet Connection Demo Web Interface Demo

    To start the Telnet demo click on the link located below. This will load the Telnet application on your system.
    »Click here to begin Telnet Demo
    At the authentication page, enter the following:
    Username: admn
    Password: admn
    Press 'Enter'

    Because the Telnet applications differ between operating systems, these instructions are designed to cover the basic operations required to make this demo operate properly.  General recommendations for all Telnet applications include having the Terminal Preferences set to VT-100/ANSI emulation and VT 100 Arrows.

    To get a display of available commands, just press Enter at the 'Switched' prompt, which will show: 

    Switched CDU Commands are:

    ON OFF REBOOT STATUS UPSTAT VERSION CREATE SHOW
    REMOVE LOGIN SET ADD DELETE LIST PASSWORD SYSSTAT
    ISTAT ENVMON LOGOUT RESTART PING CONNECT


     

     

     

     


    To view the status of all the outlets, type 'status' at the 'Sentry:' prompt.
    To turn an outlet off, type 'off' and the Outlet ID at the 'Sentry:' prompt. Example: off .a1
    To end a session type LOGOUT and press Enter.

    Please note that changes made during the demo session may NOT be preserved when the session is ended.

     

     

     

  •