(Reno, NV) July 28, 2006 -- Frost & Sullivan selected Server Technology Incorporated as the recipient of the 2006 Frost & Sullivan Award for Competitive Growth Strategy in recognition of its ability to recognize customer needs and products demands and execute an innovative product strategy within the existing competitive landscape of the power distribution unit market.
Server Technology’s Sentry™ family of Basic, Metered, Smart and Switched Cabinet Power Distribution Units (CDU’s), -48 VDC products and the Fail Safe Transfer Switch are all designed to reduce downtime and improve data center power management. Sentry products are suitable for all types of facilities from wiring closets in remote branch offices to high-power, high-density three-phase power equipment cabinets in enterprise data centers.
In addition to power management and control where the user can lock-out specific outlets or reboot remote devices that are not responding, Server Technology products provide an integral web based interface for simple user access. Another valuable feature is environmental monitoring, where multiple measurements of both temperature and humidity provide both remote monitoring and notification when a problem arises. The company is also launching a new generation of rack mount Fail Safe Transfer Switches (FSTS) to ensure redundant fail-safe power to single cord devices.
"The growth in IT and Telecom infrastructure increases the importance of remote monitoring. This technology is likely to drive the PDU market in the future also. The FSTS launched by Server Technology is anticipated to create a major breakthrough in the Transfer Switches market." Quotes Frost & Sullivan Research Analyst Suba Swaminathan.
The company offers a complete line of Basic, Metered, Smart, and Switched PDU’s for the data center cabinet along with -48 VDC products for the Telecom industry and a Fail Safe Transfer Switch product family for fail-safe redundant power applications. This "one-stop" shopping approach is unique to the CDU marketplace and very convenient for its customers as they only have one vendor to communicate with when purchasing all of their power distribution needs. It has the largest Engineering group dedicated
to the CDU market place and can often anticipate customer needs through close customer contact and product innovation.
Server Technology is very market focused and designs and manufacturer’s custom products, OEM products and private label products for the CDU market place, other CDU suppliers and the technology sector. Custom design prototypes can often be provided in as little as three weeks. Superior customer support is provided with the technical support representatives also being the same contact person that repairs the units and visit customers on field support calls.
"Server Technology keeps track of the changing needs of the customers. Their R& D infrastructure and expertise facilitate them to offer products with superior technology and desirable features which helps them to cater to their markets effectively." Quotes Frost & Sullivan Research Analyst Suba Swaminathan.
Server Technology is ISO 9001 certified and all products include agency approvals to the EN 60950-1 standard as well as the CE Mark. The company is committed to the European marketplace and offers RoHS compliant products.