Modular 3-Phase Power Distribution
Modular 3-Phase Power Distribution
Flexible and Smart Power Distribution - Simple distribution of 3-Phase Power when and where it is needed.
(Reno, NV), June 28, 2007 – Server Technology, the industry leader for Power Distribution Unit and Management Solutions, announced today that it has released a new Modular 3-phase Power Distribution product. The Sentry™ Modular Cabinet Power Distribution Unit (CDU) family is designed to take a 3-phase in-feed and distribute single phase power via Basic Cabinet PDU’s that can be placed anywhere in the cabinet. Each Basic PDU has an associated LED meter for simple load balancing. The Master unit contains the LED meters, one temperature/humidity probe input, serial connection, IP connection and exclusive link port to connect an expansion CDU for linking CDU’s on different power circuits together.
Smart Modular products allow the use of a secure network interface to view current, power, temperature and humidity levels via a web browser or Enterprise View® software as well as receiving SNMP based alarms and email alerts when thresholds are exceeded.
High density, blade server, power requirements in today’s Datacenter environments have led to new and innovative solutions for providing cabinet level power utilizing modular Cabinet PDU’s. A single power in-feed of 3-Phase 208 V 30/60 A or 400 V 32 A can provide from 10.8 to 22.2 kW of power to the cabinet. For greater densities or for redundancy dual in-feeds can be provided with two modular units linked together under one IP address providing anywhere from 21.6 to 44.4 kW of power delivered to the cabinet.
Vertical, Zero U mounting on the side or back of the cabinet ensures that valuable U space in not taken up by this Modular PDU as well as ensuring that the unit does not block airflow and also helping with the cable management.
IP Access and Security includes: Web interface, SSL, SSH, Telnet, SNMP, FTP, SNTP, Syslog, LDAP, LDAPS, TACACS+ and serial RS-232 access.
Server Technology, Inc., designs and manufactures intelligent power distribution products for enterprise data centers, service providers and branch office locations. Founded in 1984, Server Technology is recognized as a leader in innovative Remote Power Management solutions. The company’s line of Sentry™ power products eliminates unnecessary trips to remote locations and minimizes the impact of locked-up internetworking equipment on business critical networks, combining intelligent power distribution, remote management and power measurement. Server Technology is located in Reno, Nevada and can be reached at (800) 835-1515, or on the Web at www.servertech.com.
About Server Technology:
Server Technology, Inc., designs and manufactures intelligent power distribution products for enterprise data centers, service providers and branch office locations. Founded in 1984, Server Technology is recognized as a leader in innovative Remote Power Management solutions. The company’s line of Sentry™ power products eliminates unnecessary trips to remote locations and minimizes the impact of locked-up internetworking equipment on business critical networks, combining intelligent power distribution, remote management and power measurement. Server Technology is located in Reno, Nevada and can be reached at (800) 835-1515, or on the Web at www.servertech.com.
NOTE TO EDITORS: High-resolution images are available for publication. Please email Calvin Nicholson at calvin.nicholson@servertech.com for more information.
Calvin Nicholson, Marketing Manager
calvin.nicholson@servertech.com
Server Technology Inc.
www.servertech.com
1-800-835-1515