Interop® Las Vegas 2008 and Interop New York 2008 Powered by Server Technology's Cabinet Power Distribution Units (PDUs)
Interop® Las Vegas 2008 and Interop New York 2008 Powered by Server Technology's Cabinet Power Distribution Units (PDUs)
Server Technology's complete line of PDU's, Fail Safe Transfer Switches and -48 VDC products can be seen at Interop Las Vegas, booth number #2325.
(Reno, NV) March 27, 2008 - Server Technology Inc. announced today that the company will be the exclusive provider for Power Distribution Units (PDU’s) of the InteropNet event network at Interop ® Las Vegas 2008, produced by CMP Technology.Interop Las Vegas 2008 will be held April 29th to May 1st at the Mandalay Convention Center. For a complete schedule or all educational sessions, keynote addresses and participating exhibitors, visit www.interop.com. Server Technology’s complete line of PDU’s, Fail Safe Transfer Switches and -48 VDC products can be seen at Interop Las Vegas, booth number #2325.
The InteropNet network, built to support voice, video, and data for thousands of demanding attendees and sponsoring exhibitors, will be powered by Server Technology’s cabinet PDU’s which provide remote configuration and management with power distribution and power and environmental monitoring.
The InteropNet is built in collaboration with leading vendors and hand-selected products that are ready to meet any network challenge. Server Technology’s products provide a secure web based GUI, logging, Syslog support, email notification, SNMP traps, LDAP and LDAPS, TACACS+, Telnet, and out of band serial access for secure PDU access, communications and control. Environmental monitoring and control is also available along with power information such as input feed watts and system watts per square foot of the cabinet.Sentry™ Switched Cabinet Power Distribution Unit (CDU) products are also capable of communicating with Avocent’s DSView® 3 management software. Customers that select the DSView 3 management software can take advantage of a single interface for remotely and securely managing their PDU’s along with servers and serial devices making complex network access and control remarkably easy.
Interop Las Vegasattendees will have the opportunity to take free, engineer-led tours of the InteropNet throughout the exhibition and gain a practical, behind the scenes view.Tours start at the InteropNet NOC with tours scheduled daily.
The Sentry Cabinet Distribution Units (CDU’s) were the first family of cabinet-level power distribution units to provide 30-amp power distribution (110V and 208V, 208V 3-Phase) directly to the equipment cabinet while providing Branch Circuit Protection within the CDU. The Sentry CDU’s are also the first power distribution units to meet the stringent requirements of the National Electric Code (NEC) and Underwriters Laboratories (UL) 60950-1, which is now required of all new 30-amp rack-level PDUs.
For 23 years, Interop ®, part of the CMP Technology family of global brands, has helped IT and business decision-makers bring together the key components of a solid information strategy to drive efficiency and competitive advantage for their organizations.As business continues to drive the adoption of technology, and the converged network is creating new advantages, an emerging “IP for business” philosophy has woven itself into the fabric of business process applications that will be on display at Interop 2007 global events. Through in-depth educational programs, workshops, real-world demonstrations and live technology implementations in its unique InteropNet and InetropLabs programs, Interop ® provides the forum for the most powerful innovations and solutions the industry has to offer. 2007 Interop events include Interop Las Vegas, May 20-25, Mandalay Bay Convention Center; Interop Moscow, May 30-31, Forum Hal; Interop Tokyo, June 11-15, Mukahari Messe; Interop New York, October 22026, Javits Convention Center; and Interop Berlin, November 6-8, Fairground Berlin.For more information about these events, visit www.Interop.com.
About Server Technology:
Server Technology, Inc. designs and manufactures intelligent power distribution products for enterprise data centers, service providers and branch office locations. Founded in 1984, Server Technology is recognized as a leader in innovative Remote Power Management solutions. The company’s line of Sentry™ power products eliminates unnecessary trips to remote locations and minimizes the impact of locked-up internetworking equipment on business critical networks, combining intelligent power distribution, remote management and power measurement. Server Technology is located in Reno, Nevada and can be reached at (800) 835-1515, or on the Web at www.servertech.com.
NOTE TO EDITORS: High-resolution images are available for publication.Please email Calvin Nicholson at calvin.nicholson-at-servertech.com for more information.
Contact:
Calvin Nicholson, Director of Product Marketing
calvin.nicholson@servertech.com
Server Technology Inc.
www.servertech.com
1-800-835-1515